2020-12-06 11:09 PM
Hi,
We integrated en.x-cube-classb-v2-3-0 package in my application. Which is actually failing in runtime CRC test. I reduced the block size, which is actually 64 and I changed to 4 #define STEPS_NUMBER ((uint32_t)ROM_SIZE/4u) and added some code in the STL_crc32Run(void). Is modification in STL library allowed? As I reduced the block size time taken to complete CRC test is increased? Is there any time constrain to complete CRC test?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.