2022-10-15 11:08 AM
My setup is STM32H745I-DISCO board with VBAT connected to a 3V2 battery (solder bridge removed).
Here's my clock configuration:
When I set up the date and time with my UI and then watch how it ticks in real time - nothing happens. I mean - it holds time without problems.
Then I power the device off, wait a minute or two, power it back again - the time lags exactly 1 second. I repeated the test a couple of times, each time losing a second. Then I tried just resetting the device - it seems to work exactly the same - a second "eaten", so the lag increases each restart.
What's interesting, when the timer IRQs were set to 5 priority (like I wanted to call RTOS functions from ISRs) - the clock seemed to not work properly at all, it was hardly ticking. So I removed RTOS priority and set RTC IRQ to zero priority and it doesn't lag during normal device operation.
My question: how to remove the restart lag beside just pushing the clock forward one second on each start? Is there something in HAL I should check?
2022-10-15 2:10 PM
2022-10-15 11:53 PM
Thanks, so it's a known issue, I should add a conditional initialization - when the date is set I skip rest of the register setting and it should work.
HAL_StatusTypeDef HAL_RTC_Init(RTC_HandleTypeDef *hrtc)
{
HAL_StatusTypeDef status = HAL_ERROR;
/* Check RTC handler */
if(hrtc != NULL)
{
if (hrtc->Instance->DR > 0) // FIX: Seconds lost on reset.
{
hrtc->State = HAL_RTC_STATE_READY;
return HAL_OK;
}
// ... the rest of the original code...
}
}I added this fix and it seems to do the job. The clock keeps the time on restarts. Should I check something else? BTW, my app sets date, it is very important, because the date is used for filesystem operations and time-stamping data.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.