2023-01-24 1:07 AM
Hi,
I am developing an application with one configuration descriptor & 2 interfaces with 2 endpoints each. The endpoint (CUSTOM_HID) that comes as default while setting up the project via cubeIDE seems to be working alright. I can send and receive data correctly in this interface.
But when I add another interface with two of its new endpoints, the transmission (from device to host) using the in endpoint does not work & generates a pipe error on linux (libusb). Any idea why this could be occuring? Do I need to enable the macro indicating that I want to make the USB device a composite one?
Thanks
2023-01-27 7:20 AM
Hello @amankumbhani,
Please take a look at this libusb training video, it might be helpful
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.