2023-03-26 9:21 PM
2023-03-26 9:27 PM
These are the pinout and clock config diagram
I am working with STM32F407 to write a text file to Pen drive (USB Host).
f_open(&MyFile, "testfile.txt", FA_CREATE_ALWAYS | FA_WRITE);getting FD_DISC_ERR. When I debugged more i understood that this is due to HOST_DEV_WAIT_FOR_ATTACHMENT issue. Can anyone help why this is happening?
2023-03-28 4:07 AM
Hello @Ajithkumar and welcome to the Community :)
Try ClockDiv with 2 or 4.
I advise you to get inspired from the available examples available with STM32CubeF4 MCU package, and you will find more details on this article: Introduction to USB with STM32.
Make sure to use latest versions of STM32CubeMX and STM32CubeF4 MCU package.
Imen
2023-03-30 9:50 PM
Not worked. I tried with multiple clock vales.
I tried with example project in CudeIDE as well as i created new project from scratch but not worked me both.
Is any Size limitation for Flash Drive size ?
I mean I tried with 16GB and 32GB Flash Drive
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.