2021-05-23 4:10 AM
Hi to all,
I need to update from FatFS from R0.11 to R0.12c
In R0.12c there are new implementations compared to 0.11.
I see that for the STM32F401 the FATFS is in version 0.12c.
Is there a way to update the library for the STM32F103 as well?
Thank you.
Solved! Go to Solution.
2021-05-23 6:27 AM
Both are still rather stale.
Older versions should be easy enough to substitute. Replace all the middleware files, and review the settings and match those up.
The newer version s (0.13 / 0.14) will take more effort to adjust the DISKIO layer.
Use a merge tool to understand the differences
2021-05-23 6:27 AM
Both are still rather stale.
Older versions should be easy enough to substitute. Replace all the middleware files, and review the settings and match those up.
The newer version s (0.13 / 0.14) will take more effort to adjust the DISKIO layer.
Use a merge tool to understand the differences
2021-07-04 8:56 AM
HI,
Thanks for your help.
substitute folder in repository works fine ( a part that Cube MX continue in use old ffconf.h, I need to update file every time I regenerate project in Cube MX).
Now I'm facing a hardFault every time was called function validate() in f_Write().
Other fuction works fine: I'm able to mount FAT and create a file.
This is independent of what versione of FATFS I use.
I'm investigating on why hardfault are generated. Someone have some suggestions?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.