2019-05-08 3:25 AM
Hi,
is there a way to program a STM32 Nucleo board (Nucleo-F767ZI) via the Ethernet interface?
The problem with the usb port is when the Nucleo 5V is powered externally via the E5V pin, at power on of the 5V, the usb cable must be removed. So on a remote system someone has to connect the usb cable first before I can program the Nucleo. So if I can program the Nucleo via the Ethernet interface, I can avoid this problem.
Best regards,
Luc
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.