2022-04-05 3:32 AM
Hi everybody,
I am working with AZURE RTOS and I have implemented an HTTP web server application. I started from the example available in CubeIDE. Everything is working properly but now I need to modifiy the HTTP web page. For this, it is necessary to generate a .bin file from the .js, .css and .html files:
Could somebody help me with this issue? I think it should exists a script or something like that for it.
Thanks in advance.
Solved! Go to Solution.
2022-04-07 1:57 AM
Hi,
In this case I think you may find this thread interesting:
Have a look at Vangelis answer...
2022-04-06 2:14 AM
Hi,
Did you start from:
X-CUBE-AZRTOS-H7\2.0.0\Projects\STM32H735G-DK\Applications\NetXDuo\Nx_WebServer
If relying on the above example then you are storing the webpage on an SD-card, relying on FileX... No bin-file should be needed.
So, I assume you are based on another example?
2022-04-06 2:39 AM
Hi,
I started from:
X-CUBE-AZRTOS-F4\1.0.0\Projects\STM32F429ZI-Nucleo\Applications\NetXDuo\Nx_WebServer
Then, it is necessary to store the binary in the flash memory. Actually that is the best solution for my project as I don't have SD-card reader (LevelX is used as well).
Thanks.
2022-04-07 1:57 AM
Hi,
In this case I think you may find this thread interesting:
Have a look at Vangelis answer...
2022-04-07 3:37 AM
Thank you so much. Something like that is just what I was testing. A perl script.
2022-04-19 8:33 AM
I'm still trying to generate the web files for flash memory. web_content.bin (from web server example) has been generated in any way and I would like to know it. Does somebody know something about it?
2023-02-24 7:53 AM
Does someone know how it is created the file web_demo.bin in the Nx_WebServer example for the board STM32F429ZI-Nucleo?
I have seen that web_demo.bin is divided in sector of 1024 bytes and the data are written in the first 532 (512 effective data + 20) bytes of the sector.
Any Idea?
Thanks
2023-04-10 9:05 PM
Just in case you are still looking for a solution, here is a script to generate raw FAT disk.
github.com/TiejunMS/utils/tree/main/scripts/gen_raw_disk
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.