2025-09-15 12:15 AM
void HAL_SMBUS_ErrorCallback(SMBUS_HandleTypeDef* SMBUSHandle)
{
/** Error_Handler() function is called when error occurs.
* 1- When Slave doesn't acknowledge its address, Master restarts
* communication. 2- When Master doesn't acknowledge the last data
* transferred, Slave doesn't care in this example.
*/
if (HAL_SMBUS_GetError(SMBUSHandle) != HAL_SMBUS_ERROR_ACKF)
{
printf("failed\r\n");
/* Turn Off LED2 */
}
}
/**
* @brief Slave Address Match callbacks.
* hsmbus : Pointer to a SMBUS_HandleTypeDef structure that contains
* the configuration information for the specified SMBUS.
* @retval None
*/
void HAL_SMBUS_AddrCallback(SMBUS_HandleTypeDef* hsmbus, uint8_t TransferDirection, uint16_t AddrMatchCode)
{
SlaveAddrMatchCode = (AddrMatchCode << 1);
HAL_SMBUS_EnableListen_IT(&hsmbus1);
uint8_t tx_buff = 0x00;
HAL_SMBUS_Slave_Transmit_IT(&hsmbus1, &tx_buff, 1, SMBUS_FIRST_AND_LAST_FRAME_WITH_PEC);
// HAL_SMBUS_Slave_Transmit_IT(&hsmbus1, &aTxBuffer, 1,
// SMBUS_FIRST_AND_LAST_FRAME_WITH_PEC);
UNUSED(TransferDirection);
}
void HAL_SMBUS_SlaveRxCpltCallback(SMBUS_HandleTypeDef* hsmbus)
{
HAL_SMBUS_Slave_Receive_IT(&hsmbus1, dummy_data, 2, SMBUS_FIRST_AND_LAST_FRAME_WITH_PEC);
}
//
// return 0;
//}
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick.
*/
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART3_UART_Init();
MX_USART2_UART_Init();
MX_TIM1_Init();
MX_I2C1_SMBUS_Init();
MX_I2C3_SMBUS_Init();
/* USER CODE BEGIN 2 */
/* Enable the Analog SMBUS Filter */
HAL_SMBUS_ConfigAnalogFilter(&hsmbus1, SMBUS_ANALOGFILTER_ENABLE);
/* Enable address Match detect with interrupt */
HAL_SMBUS_EnableListen_IT(&hsmbus1);
/* Wait until address matched */
while (SlaveAddrMatchCode != SMBUS_ADDRESS)
;
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
Solved! Go to Solution.
2025-09-15 1:32 AM
Hello @suguresh_m ,
I recommend downloading the X-CUBE-SMBUS Expansion Package, which contains the SMBus/PMBus® stack implementation for STM32Cube. This package provides example projects and basic functionality tests for the following boards: NUCLEO-G431RB ,NUCLEO-H743ZI,NUCLEO-L4R5ZI & NUCLEO-WB55RG ...
You can download the package directly from ST's official website here:
https://www.st.com/en/embedded-software/x-cube-smbus.html
Additionally, I suggest reviewing the related Application Note for detailed guidance:
https://www.st.com/resource/en/application_note/an4502-stm32-smbuspmbus-expansion-package-for-stm32cube-stmicroelectronics.pdf
This resource should be very helpful in resolving your issue.
Br
2025-09-11 10:00 PM - last edited on 2025-09-12 12:37 AM by Peter BENSCH
Edited by ST moderator to be inline with the community rules especially with the code sharing. In next time please use </> button to paste your code. Please read this post: How to insert source code.
void HAL_SMBUS_ErrorCallback(SMBUS_HandleTypeDef* SMBUSHandle)
{
/** Error_Handler() function is called when error occurs.
* 1- When Slave doesn't acknowledge its address, Master restarts
* communication. 2- When Master doesn't acknowledge the last data
* transferred, Slave doesn't care in this example.
*/
if (HAL_SMBUS_GetError(SMBUSHandle) != HAL_SMBUS_ERROR_ACKF)
{
printf("failed\r\n");
/* Turn Off LED2 */
}
}
/**
* @brief Slave Address Match callbacks.
* hsmbus : Pointer to a SMBUS_HandleTypeDef structure that contains
* the configuration information for the specified SMBUS.
* @retval None
*/
void HAL_SMBUS_AddrCallback(SMBUS_HandleTypeDef* hsmbus, uint8_t TransferDirection, uint16_t AddrMatchCode)
{
SlaveAddrMatchCode = (AddrMatchCode << 1);
HAL_SMBUS_EnableListen_IT(&hsmbus1);
uint8_t tx_buff = 0x00;
HAL_SMBUS_Slave_Transmit_IT(&hsmbus1, &tx_buff, 1, SMBUS_FIRST_AND_LAST_FRAME_WITH_PEC);
// HAL_SMBUS_Slave_Transmit_IT(&hsmbus1, &aTxBuffer, 1,
// SMBUS_FIRST_AND_LAST_FRAME_WITH_PEC);
UNUSED(TransferDirection);
}
void HAL_SMBUS_SlaveRxCpltCallback(SMBUS_HandleTypeDef* hsmbus)
{
HAL_SMBUS_Slave_Receive_IT(&hsmbus1, dummy_data, 2, SMBUS_FIRST_AND_LAST_FRAME_WITH_PEC);
}
//
// return 0;
//}
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick.
*/
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART3_UART_Init();
MX_USART2_UART_Init();
MX_TIM1_Init();
MX_I2C1_SMBUS_Init();
MX_I2C3_SMBUS_Init();
/* USER CODE BEGIN 2 */
/* Enable the Analog SMBUS Filter */
HAL_SMBUS_ConfigAnalogFilter(&hsmbus1, SMBUS_ANALOGFILTER_ENABLE);
/* Enable address Match detect with interrupt */
HAL_SMBUS_EnableListen_IT(&hsmbus1);
/* Wait until address matched */
while (SlaveAddrMatchCode != SMBUS_ADDRESS)
;
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
2025-09-11 11:12 PM
Please provide me a solution with SMBUS In SLAVE configuration without PEC or with PEC
2025-09-15 1:32 AM
Hello @suguresh_m ,
I recommend downloading the X-CUBE-SMBUS Expansion Package, which contains the SMBus/PMBus® stack implementation for STM32Cube. This package provides example projects and basic functionality tests for the following boards: NUCLEO-G431RB ,NUCLEO-H743ZI,NUCLEO-L4R5ZI & NUCLEO-WB55RG ...
You can download the package directly from ST's official website here:
https://www.st.com/en/embedded-software/x-cube-smbus.html
Additionally, I suggest reviewing the related Application Note for detailed guidance:
https://www.st.com/resource/en/application_note/an4502-stm32-smbuspmbus-expansion-package-for-stm32cube-stmicroelectronics.pdf
This resource should be very helpful in resolving your issue.
Br
2025-09-15 6:42 AM
Hello @suguresh_m
An example of an SMBus receive implementation is provided below.
#include "stm32xxxx_hal.h" // Replace with your specific device header
// --- Global Variables ---
SMBUS_HandleTypeDef SmbusHandle;
uint8_t RxBuffer[NUMDATA]; // Define NUMDATA as needed
uint16_t Smbus_adresse = 0xXX; // Set your slave address here
uint16_t SlaveAddrMatchCode = 0;
// --- Function Prototypes ---
void SystemClock_Config(void);
void Error_Handler(void);
// --- Main Function ---
int main(void)
{
HAL_Init();
SystemClock_Config();
// Initialize SMBUS
HAL_SMBUS_Init(&SmbusHandle);
// Enable Listen mode with interrupt
if (HAL_SMBUS_EnableListen_IT(&SmbusHandle) != HAL_OK)
{
Error_Handler();
}
// Main loop
while (1)
{
// Your main code here
}
}
// --- Address Match Callback ---
void HAL_SMBUS_AddrCallback(SMBUS_HandleTypeDef *hsmbus, uint8_t TransferDirection, uint16_t AddrMatchCode)
{
SlaveAddrMatchCode = (AddrMatchCode << 1);
if (SlaveAddrMatchCode == Smbus_adresse)
{
// Start receiving data in interrupt mode
if (HAL_SMBUS_Slave_Receive_IT(hsmbus, RxBuffer, NUMDATA, SMBUS_FIRST_AND_LAST_FRAME_WITH_PEC) != HAL_OK)
{
Error_Handler();
}
}
}
// --- Error Handler ---
void Error_Handler(void)
{
// User can add error handling here
while (1)
{
// Stay here
}
}
// --- System Clock Configuration ---
// Implement this function as per your MCU and application requirements
void SystemClock_Config(void)
{
// System clock configuration code
}
2025-09-15 8:11 AM
im receiving 5pckets to read and write means vise versa once i get some data i need to reply with some data. but its not synchronizing. i tried lot of example but timing issues unable to handle
2025-09-15 8:13 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.