2024-05-07 11:57 PM
Hi all,
I config the SDIO & FATFS by cubeMx for my STM32F429BI board.
When I config the SDIO to SDIO_BUS_WIDE_1B, everything is work well; Even the generated MX_SDIO_SD_Init() is NOT calling the HAL_SD_Init() function. (Why don't need HAL_SD_Init() , is this some mistake?)
void MX_SDIO_SD_Init(void)
{
HAL_StatusTypeDef hal_sta;
hsd.Instance = SDIO;
hsd.Init.ClockEdge = SDIO_CLOCK_EDGE_RISING;
hsd.Init.ClockBypass = SDIO_CLOCK_BYPASS_DISABLE;
hsd.Init.ClockPowerSave = SDIO_CLOCK_POWER_SAVE_DISABLE;
hsd.Init.BusWide = SDIO_BUS_WIDE_1B;
hsd.Init.HardwareFlowControl = SDIO_HARDWARE_FLOW_CONTROL_DISABLE;
hsd.Init.ClockDiv = 0;
}
However, when I change SDIO_BUS_WIDE_1B to SDIO_BUS_WIDE_4B, the operate to SD card is error.
But when I change the code to below, the program works well again:
void MX_SDIO_SD_Init(void)
{
HAL_StatusTypeDef hal_sta;
hsd.Instance = SDIO;
hsd.Init.ClockEdge = SDIO_CLOCK_EDGE_RISING;
hsd.Init.ClockBypass = SDIO_CLOCK_BYPASS_DISABLE;
hsd.Init.ClockPowerSave = SDIO_CLOCK_POWER_SAVE_DISABLE;
hsd.Init.BusWide = SDIO_BUS_WIDE_1B;
hsd.Init.HardwareFlowControl = SDIO_HARDWARE_FLOW_CONTROL_DISABLE;
hsd.Init.ClockDiv = 0;
hal_sta = HAL_SD_Init(&hsd);
if(hal_sta != HAL_OK) {
LOG_ERR("SD init err[%d]\n", hal_sta);
}
hal_sta = HAL_SD_ConfigWideBusOperation(&hsd, SDIO_BUS_WIDE_4B);
if(hal_sta != HAL_OK) {
LOG_ERR("SD configWideBus err[%d]\n", hal_sta);
} else {
LOG_DBG("SD configWideBus to 4bit ok\n");
}
}
I can't understand what the difference to config the BusWide between HAL_SD_Init() and HAL_SD_ConfigWideBusOperation();
Could someone can explain it, thank you!
Solved! Go to Solution.
2024-05-08 1:29 AM
Hello,
What you did is correct and this is what you supposed to do.
Please refer to that thread:
2024-05-08 1:29 AM
Hello,
What you did is correct and this is what you supposed to do.
Please refer to that thread:
2024-05-08 8:06 AM - edited 2024-05-08 8:13 AM
Hello @Junde
The function HAL_SD_Init() is responsible for the initial setup of the SDIO using the STM32 HAL library. It calls HAL_SD_InitCard(), which configures the SDIO peripheral with default settings for the first initialization. Here is a snippet of the HAL_SD_InitCard() function:
HAL_StatusTypeDef HAL_SD_InitCard(SD_HandleTypeDef *hsd)
{
uint32_t errorstate;
HAL_StatusTypeDef status;
SD_InitTypeDef Init;
/* Default SDIO peripheral configuration for SD card initialization */
Init.ClockEdge = SDIO_CLOCK_EDGE_RISING;
Init.ClockBypass = SDIO_CLOCK_BYPASS_DISABLE;
Init.ClockPowerSave = SDIO_CLOCK_POWER_SAVE_DISABLE;
Init.BusWide = SDIO_BUS_WIDE_1B;
Init.HardwareFlowControl = SDIO_HARDWARE_FLOW_CONTROL_DISABLE;
Init.ClockDiv = SDIO_INIT_CLK_DIV;
/* Initialize SDIO peripheral interface with default configuration */
status = SDIO_Init(hsd->Instance, Init);
if(status != HAL_OK)
{
return HAL_ERROR;
}
/* Disable SDIO Clock */
__HAL_SD_DISABLE(hsd);
/* Set Power State to ON */
(void)SDIO_PowerState_ON(hsd->Instance);
/* Enable SDIO Clock */
__HAL_SD_ENABLE(hsd);
/* Required power up waiting time before starting the SD initialization sequence */
HAL_Delay(2);
/* Identify card operating voltage */
errorstate = SD_PowerON(hsd);
if(errorstate != HAL_SD_ERROR_NONE)
{
hsd->State = HAL_SD_STATE_READY;
hsd->ErrorCode |= errorstate;
return HAL_ERROR;
}
/* Card initialization */
errorstate = SD_InitCard(hsd);
if(errorstate != HAL_SD_ERROR_NONE)
{
hsd->State = HAL_SD_STATE_READY;
hsd->ErrorCode |= errorstate;
return HAL_ERROR;
}
/* Set Block Size for Card */
errorstate = SDMMC_CmdBlockLength(hsd->Instance, BLOCKSIZE);
if(errorstate != HAL_SD_ERROR_NONE)
{
/* Clear all the static flags */
__HAL_SD_CLEAR_FLAG(hsd, SDIO_STATIC_FLAGS);
hsd->ErrorCode |= errorstate;
hsd->State = HAL_SD_STATE_READY;
return HAL_ERROR;
}
return HAL_OK;
}
To enable 4-bit wide bus operation on an SD card, you need to call the function HAL_SD_ConfigWideBusOperation() separately after initializing the card with HAL_SD_InitCard().
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.