2019-01-08 10:20 PM
I am using an STM32F031 and I can't see specific documentation for the F03x type. All I have is F070, F072 and F091 MCU types.
The Low Level API functions do not map correctly. For example, I am trying to set the PLL clock source and the function to do so is LL_RCC_PLL_ConfigDomain_SYS
All three help docs show 3 parameters for the function, whereas the actual function call for my MCU has two parameters.
Ok, it seems Doxygen is used but when I try, I can't get the output correct. For the pre-processor part, I enter the MCU part number STM32F031x6 but I don't get what I expect.
Any help with knowing what to put in the different fields, or a document somewhere that explains how ST does it would be much appreciated
Cheers
2019-05-22 5:26 PM
Bump
2019-05-22 6:01 PM
https://community.st.com/s/question/0D50X0000AFs71HSQR/user-manual
@Khouloud GARSI @Nawres GHARBI
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.