2019-04-23 10:09 PM
I was trying to upload a code on NUCLEO-F446RE board using the USB-DFU protocol. I was supposed to make the Boot 0 pin high and reset it to get the device into bootloader mode. I was able to see and access the partitions of the device neither on DfuSe Demo software on windows nor on dfu-util on linux and could successfully upload the code too but I am not able to view the partitions on a consistent basis after rebooting the device into the bootloader mode. Though after rebooting after making the BOOT 0 pin high, it is might be entering the bootloader mode as the normal functionality stops once I reboot it after making the BOOT 0 pin high (I was running a code for lighting the LED by pressing the user button which stops working after rebooted by making BOOT0 high but I am not able to see the partitions consistently neither on DfuSe nor on dfu-util ). Kindly Help.
Thanks in advance
Siddharth
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.