2023-01-12 1:39 PM
I am using 9600 baud rate and even parity .
Address bytes sent with checksum is 08 00 00 00 08 ACK Received
2023-01-18 9:35 AM
Hello @sunny123,
Could you please be more specific about NACK? Does it transmits a NACK byte or aborts the command?
Could you check if the address is valid? If yes, please provide us a dump/ log for better understanding of the issue.
You should refer to AN3155 section 3.6 Write Memory command for further details about the requirements to respect the order of the code sequence.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-01-18 10:13 AM
Provide a more complete data-gram flow, your situation is hard to understand/interpret.
My recollection of a data packet.. For FLASH use aligned addresses and perhaps 8-16 byte patterns
{ // Tx: 31 Write
BYTE data[25] = { 0x31, 0xCE, 0x20, 0x00, 0x00, 0x00, 0x20, // WRITE 0x20000000, w/SUM
0x0F, // 16 Bytes
0x00, 0x11, 0x22, 0x33, 0x44, 0x55, 0x66, 0x77, // Data pattern
0x88, 0x99, 0xAA, 0xBB, 0xCC, 0xDD, 0xEE, 0xFF,
0x0F }; // SUM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.