2018-05-01 6:22 PM
Hi Everyone,
I've been tasked with developing a bootloader to enable a device to do a firmware update via USB.
I'm sure this question has been asked in various forms many times, but I'm new to the world of STM32 and ARM and I'm having a bit of trouble putting all the information I've been finding together.
First off, I'll describe more specifically what we would like to do. We want a simple, reliable way to upgrade our devices in the field without requiring service technicians to bring chip programmers with them.
Ideally, a technician would use a hidden factory menu on the device to enable bootloader update mode, at which point the device would reboot into the bootloader and wait for the USB stick to be plugged in. After the update, the device would reboot back into the application. These devices are large appliances that could potentially be difficult to disconnect from power, so all resets would need to be initiated by the code.
Our starting point for this endeavour is the STM322xG-EVAL_USBH-FS example project. So far I've successfully modified the example to match our board layout, and I've been able to successfully flash our application from the bootloader and have it start automatically once the vector table location was updated in the application.
The current flash settings are (let me know if you need more information, the rest of the code is essentially the same as the example):
Bootloader
VECT_TAB_OFFSET 0x00
USER_FLASH_STARTADDRESS 0x08008000
APPLICATION_ADDRESS 0x08008000
Application
VECT_TAB_OFFSET 0x08008000
Application start address (linker setting) 0x08008000
However, after the bootloader flashes the app, the device will no longer go into the bootloader. To be able to run the bootloader again, I have to erase the chip (using a ST-LINK V2 programmer and the ST-LINK Utility) and reflash the bootloader. Simply reflashing the bootloader while the application is loaded still results in the application launching each time, bypassing the bootloader. I checked the bootloader size to make sure it wasn't being partially overwritten and it looks okay (bootloader size is listed as 0x58A8 by the ST-LINK Utility).
So right now my questions are:
Thanks in advance for any help and for pointing me in the right direction with this.
#bootloaderWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.