2019-09-22 3:33 PM
2019-09-23 7:26 AM
I don't know what F4 part you are using. Most only need that if you use high speed parts, like at 180 MHz, where the VCO won't divide down into 48 MHz naturally. The classic F2/F4 parts can only use the PLL-Q tap.
Perhaps looks a USB Device examples provided in the HAL for F429 or F446 type processors, if you're using those.
2019-09-22 4:41 PM
The Generic F4 pulls the 48 MHz from the Q Tap of the PLL
ie 336 / 7 = 48 where 336 / 2 = 168 from the P Tap
RCC_OscInitStruct.PLL.PLLN = 336; // VCO from 1 MHz comparison frequency, ie (HSE / M)
RCC_OscInitStruct.PLL.PLLP = 2; // CPU
RCC_OscInitStruct.PLL.PLLQ = 7; // USB
2019-09-23 7:01 AM
thanks for your reply Clive, so should i also configure the RCC_DCKCFGR2 by configuring the SDIO/USBFS clock selection bit or just clocking the RCC_AHB2Periph_OTG_FS with the AHB2 is sufficient in order to use my usb driver properly?
2019-09-23 7:26 AM
I don't know what F4 part you are using. Most only need that if you use high speed parts, like at 180 MHz, where the VCO won't divide down into 48 MHz naturally. The classic F2/F4 parts can only use the PLL-Q tap.
Perhaps looks a USB Device examples provided in the HAL for F429 or F446 type processors, if you're using those.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.