2022-11-25 6:35 AM
I'm using Keil (Scatter file, not lnker) and I have a bootloader and a place for two images (one active and other is for the over the air update).
i use Cortex M0 processor where there is no Vector Table Offset Register and i used to copy the vector table from flash to sram.
The problem here:
1. I do the ota update using the application and not using the bootloader.
2. I build the firmware for a specific location and when the ota update is happening the active application (which is in slot A) is downloading the new image in Slot B (but the image is built using the linker script for slot A).
3. When I jump from bootloader to app using the function pointer (I see the function ptr is holding the right address.)
4. But when jumping it is creating a hard fault.
5. So the image built for a specific place should only be used there? Can't I use it for other slots (I also look for page alignment)? if not what can be the possible reason for hard fault?
Solved! Go to Solution.
2022-11-25 4:17 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.