2025-07-06 11:27 PM
I’m working on a project using STM32H7 (Cortex-M7 core) with eMMC and Azure RTOS FileX to manage file systems.
The buffer is allocated as:
ALIGN_32BYTES (uint32_t fx_mmc_media_memory[FX_STM32_MMC_DEFAULT_SECTOR_SIZE / sizeof(uint32_t)]);
During initialization, I call:
fx_system_initialize();
fx_media_open(&gst_mmc_disk, "eMMC", fx_stm32_mmc_driver, ...);
However, the system crashes with a HardFault inside: SCB_InvalidateDCache_by_Addr()
which is called from: fx_media_open() ->fx_stm32_mmc_driver() ->mmc_read_data() ->invalidate_cache_by_addr()
2025-07-09 2:54 AM
Hello @Riya
Please make sur fx_mmc_media_memory is placed in a cacheable region and cache is enabled.
2025-12-16 5:48 AM
Hi Riya
Looks like I ran into the same problem you reported, did you discover a fix?
2025-12-16 6:20 AM
I experienced the same problem, and for me the solution is to enable the DCache. Enter the Stm32CubeMX (6.15.0) - Under system core, item CORTEX_M7, "Cortex Interface Settings, CPU DCache set to Enabled.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.