2016-10-27 1:27 AM
hello!
I'm using STM32f407 discovery kit along with extension board for my webserver project, I've tested lwip demo code and it works fine. Problem comes when client sends a bigger packet, for example 2000 bytes, and server receives data in segmented form, is there a way to handle multiple segments in httpd.c file? may combine two segments to make it single before processing?Thank you. #stm32f4 #lwip #httpd2016-10-27 3:53 AM
http is built over tcp so what you receive is not a ''packet'', rather, a stream. But I understand your concern - tcp serves received data to http in chunks (I am reluctant to use ''packets'' here as the relationship to IP packets is indirect) indeed. In the recv callback (http_recv()), after whatever check you may have for data-completely-arrived determines you need to wait for more data, you either store the already received data into your own local storage (array in RAM); or (a more complex but potentially RAM-saving), use pbuf_cat() to chain up the received data, not pbuf_free() them until the last portion arrived, and when that happens, processing all of them (including pbuf_free()) at once. This requires to understand the pbuf mechanisms and have enough pbufs allocated.
There is aimed at lwip users, this sort of questions might be better answered there, as they are in fact not STM32 related. JWWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.