cancel
Showing results for 
Search instead for 
Did you mean: 

HAL_I2S_TransmitDMA in circular mode (STM32H503) doesn't run continuously

chriskuku
Senior III

I have set up a DMA on an I2S device with an STM32H503CBU6. The idea is, that the DMA runs continuously on a single bufferaddress (one word, containing the left and right channels for the external I2S-DAC). When the DMA transfer of that 1 word is complete it should start over again by itself.

At present the goal is not achieved with the following setup:

uint16_t ram_loc[2] = {0,0};
int main(void)
{

  

  /* MCU Configuration--------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();



  /* Configure the system clock */
  SystemClock_Config();

 

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_GPDMA1_Init();
  MX_ICACHE_Init();
  MX_I2C1_Init();
  MX_I2S2_Init();
  MX_TIM1_Init();
  
      HAL_I2S_Transmit_DMA(&hi2s2, ram_loc,1); // since circular is configured,
                                               // am I right that the DMA keeps alive itself?
  /* USER CODE END 2 */

  /* Infinite loop */
 
     while (1)
     {

    	// for testing, increment ram_loc (L+R) by one every 10ms
    	// which should produce a (sawtooth) ramp.
    	//
    	 HAL_Delay(10);
    	 ram_loc[0]++,ram_loc[1]++;
    	 if(ram_loc[0] == 65535)
    		 ram_loc[0]=ram_loc[1]=0;
	
    }
 
}

 

Some things I'm not sure about: how is the DMA data organized. Since it is an I2S audio stream with L+R signals, I assume they are two words of 16bits, sent in one 32bit DMA chunk. Or is it 32bit data in a 32bit frame? BTW, what does "frame" actually stand for?
What is the "Port 0" that appears, when I choose "circular" mode in the DMA channel 4 setup?

I2S2_WS  - PA3
I2S2_CK  - PA5
I2S2_SDO - PB1

 I don't see any data on PB1. Timing is there (48KHz on PA5, WS on PA3).

1 ACCEPTED SOLUTION

Accepted Solutions

I got it running. I hadn't finished the necessary setup of the GPDMA.
Had to define a linked list with two nodes. And get some other parameters in the I2S interface (word length etc.) right. See attached IOC.

 

View solution in original post

8 REPLIES 8
TDK
Super User

You should initialize ram_loc with nonzero data, and make it volatile.

volatile uint16_t ram_loc[2] = {0xAAAA, 0xAAAA};

 

Clock is there. Data is probably there as well. It's not being updated because the compiler is free to optimize it away.

If you feel a post has answered your question, please click "Accept as Solution".

Would have been too nice, but:

volatile uint16_t ram_loc[2] = {0xAAAA, 0xAAAA};
../Core/Src/main.c: In function 'main':
../Core/Src/main.c:179:36: warning: passing argument 2 of 'HAL_I2S_Transmit_DMA' discards 'volatile' qualifier from pointer target type [-Wdiscarded-qualifiers]
  179 |       HAL_I2S_Transmit_DMA(&hi2s2, ram_loc,1); // since circular is configured,
      |                                    ^~~~~~~

And, thinking about it, the compiler shouldn't optimize a variable away, that is being passed to a function

and is being assigned (incremented) further down in the while loop in the code. Or am I wrong? And non-zero data? No, this can't be it. 

Data is data, whether zero or non-zero, it's an initialization.

 HAL_I2S_Transmit_DMA(&hi2s2, (uint16_t*)ram_loc,1)

Cast it to the proper type to avoid the warning.

If you feel a post has answered your question, please click "Accept as Solution".

@TDK wrote:
 HAL_I2S_Transmit_DMA(&hi2s2, (uint16_t*)ram_loc,1)

Cast it to the proper type to avoid the warning.


Did that, no change. Still no data. I'm wondering if it has to do sth. with circular and linked lists downstream in the DMA configuration in 

HAL_I2S_Transmit_DMA

 

The fact that the timing can be seen at the I2S2 pins cannot be interpreted as the DMA being running, can it?

 

I traced HAL_I2S_Transmit_DMA a bit. It runs into the following code:

  /* Enable the Tx DMA Stream/Channel */
  if ((hi2s->hdmatx->Mode & DMA_LINKEDLIST) == DMA_LINKEDLIST)
  {
    if (hi2s->hdmatx->LinkedListQueue != NULL)
    {
      /* Set DMA data size */
      hi2s->hdmatx->LinkedListQueue->Head->LinkRegisters[NODE_CBR1_DEFAULT_OFFSET] = hi2s->TxXferCount;

      /* Set DMA source address */
      hi2s->hdmatx->LinkedListQueue->Head->LinkRegisters[NODE_CSAR_DEFAULT_OFFSET] = (uint32_t)hi2s->pTxBuffPtr;

      /* Set DMA destination address */
      hi2s->hdmatx->LinkedListQueue->Head->LinkRegisters[NODE_CDAR_DEFAULT_OFFSET] = (uint32_t)&hi2s->Instance->TXDR;

      errorcode = HAL_DMAEx_List_Start_IT(hi2s->hdmatx);
    }

I'm wondering about the 

HAL_DMAEx_List_Start_IT(hi2s->hdmatx);

I cannot remember having enabled any interrupts. 

Could it be I have to add a LINKEDLIST (under Utilities in the IOC)?

I got it running. I hadn't finished the necessary setup of the GPDMA.
Had to define a linked list with two nodes. And get some other parameters in the I2S interface (word length etc.) right. See attached IOC.

 

For clarification's sake, after defining the linked list, did you implement them the way specified in this tutorial?
I have to ask since, from my own tests and your IOC, I'm guessing that circular DMA, even in Standard Request Mode, still requires a setup similar to the Linked List Mode in the newer DMA controllers.

Thank you in advance, this thread was very useful, even for the H7RS I'm using right now.

Hi, thanks for your comments. I believe, I was using a YT video for getting inspiration, not the link you are refering. But that one is also interesting.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.