2018-04-18 2:23 AM
I'm trying to use the I2C slave in DMA mode.
uint8_t aRxBuffer;
HAL_I2C_Slave_Receive_DMA(&hi2c1, (uint8_t*)&aRxBuffer, 1);But HAL_I2C_Slave_Receive_DMA returns HAL_BUSY.
At the same time I have no other devices on the bus.
SDA and SCL pulling to VIO
Init code:
static void MX_I2C1_Init(void) {
hi2c1.Instance = I2C1; hi2c1.Init.ClockSpeed = 400000; hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_16_9; hi2c1.Init.OwnAddress1 = 0x20 << 1; hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT; hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE; hi2c1.Init.OwnAddress2 = 0; hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE; hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE; if (HAL_I2C_Init(&hi2c1) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); }}#i2c-slave #hal_i2c2018-08-10 9:19 AM
Sorry, bumping old zombie unanswered threads off my feed
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.