2025-08-29 10:43 PM - edited 2025-08-29 10:44 PM
Hi everyone,
I am currently running the DCMIPP_Continuous mode example from STM32N6Cube firmware v1.2.0. However, I am getting stuck at the function call:
HAL_result = HAL_RCC_OscConfig(&RCC_OscInitStruct);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_NONE;
RCC_OscInitStruct.PLL1.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL1.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL1.PLLM = 4;
RCC_OscInitStruct.PLL1.PLLN = 75;
RCC_OscInitStruct.PLL1.PLLFractional = 0;
RCC_OscInitStruct.PLL1.PLLP1 = 1;
RCC_OscInitStruct.PLL1.PLLP2 = 1;
RCC_OscInitStruct.PLL2.PLLState = RCC_PLL_NONE;
RCC_OscInitStruct.PLL3.PLLState = RCC_PLL_NONE;
RCC_OscInitStruct.PLL4.PLLState = RCC_PLL_NONE;
HAL_StatusTypeDef HAL_result; // Have a variable to catch the result
HAL_result = HAL_RCC_OscConfig(&RCC_OscInitStruct); // Catch the result
if (HAL_result != HAL_OK)
{
Error_Handler();
}After some debugging, I found that the function returns HAL_ERROR. Earlier, this code was working fine, but now it consistently fails at this point.
Could anyone please guide me on how to proceed with this issue?
Thanks in advance!
Solved! Go to Solution.
2025-11-14 9:24 PM - edited 2025-11-20 9:21 PM
Solution -
Even I am not sure about this but apparently when my default IMX335 camera is connected (just cable attached) to the board it doesn't configure the clock. After removing it, it works properly.
Strangely (while camera attached) even LED blink example doesn't run even though the camera is not being configured.
2025-08-30 9:01 AM
Hi,
(I dont have an N6 , but ..)
OscillatorType = RCC_OSCILLATORTYPE_NONE;
this is correct ? type none ?
2025-09-02 1:34 AM
@athern27 wrote:
Earlier, this code was working fine, but now it consistently fails at this point.
You mean it was working in previous version?
2025-11-14 9:24 PM - edited 2025-11-20 9:21 PM
Solution -
Even I am not sure about this but apparently when my default IMX335 camera is connected (just cable attached) to the board it doesn't configure the clock. After removing it, it works properly.
Strangely (while camera attached) even LED blink example doesn't run even though the camera is not being configured.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.