cancel
Showing results for 
Search instead for 
Did you mean: 

H743_EVAL USB_HOST/HID_Standalone example.

Asantos
Senior

The main loop of the HID_Standalone example is:

while(1)

{

USBH_Process(&USBHost);

HID_MenuProcess();

}

The problem is when a slow process is put in the loop:

while(1)

{

HAL_Delay(10); //or any slow process > 8ms

USBH_Process(&USBHost);

HID_MenuProcess();

}

In this case the USB host stop receiving keyboard characters.

Just one occurrence of a process or delay with more than 8 ms in the loop causes permanent failure in the process of receiving characters typed from the keyboard.

How keep the delay and USBHost working?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
CopaCabana_ Reemer
Associate II

@note Care must be taken when using HAL_Delay(), this function provides accurate delay (in milliseconds)

based on variable incremented in SysTick ISR. This implies that if HAL_Delay() is called from

a peripheral ISR process, then the SysTick interrupt must have higher priority (numerically lower)

than the peripheral interrupt. Otherwise the caller ISR process will be blocked.

To change the SysTick interrupt priority you have to use HAL_NVIC_SetPriority() function.

information of this applicaiton.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.