2021-12-07 7:50 AM
Hi,
After installing the x-cube-aws demo software, when I turn on the board, the following error occurs.
>>>
.........................
Module initialized successfully: Inventek eS-WiFi ISM43362-M3G-L44-SPI C3.5.2.5.STM
Retrieving the WiFi module MAC address: c4:xx:xx:xx:xx:1f
Connecting to AP: e4ds_studio Attempt 1/3 ...
Connected to AP e4ds_studio
Mac address: c4:xx:xx:xx:xx:xx
Retrieving the IP address.
IP address: 172.xx.x.xx
Push the User button (Blue) within the next 5 seconds if you want to update the device security parameters or credentials.
Setting the RTC from the network time.
ERROR: net_sock_open_mbedtls L#165 failed
! mbedtls_x509_crt_parse returned -0x2180 while parsing root cert
ERROR: setRTCTimeDateFromNetwork L#134 Could not open the socket.
Error initializing the RTC from the network time!
2022-01-10 1:13 AM
Could you create a new question about your GCP problem in Q&A / STM32 MCUs ?
as we are discussing GCP it's not the same as the original poster issue.
2022-01-12 1:33 AM
Thank you guys
I finished the test of the 'STM32L4 discovery kit iot nano board' by connecting it to Microsoft Azure.
I will try again according to your advice to connect with AWS.
2022-01-12 7:15 AM
Hello @BSalt.1
When you tried the STM32L4 IoT kit board to connect to Microsoft Azure, did it work straight away ? if not, what solved the problem ?
2022-01-13 3:41 AM
@Guillaume K
Hi,
Yes, I followed the following link, it connected very well.
https://docs.microsoft.com/en-us/azure/iot-develop/quickstart-devkit-stm-b-l475e
All tests went smoothly.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.