2023-09-01 2:23 PM
The example does not work. It times out:
Stack:
HAL_OSPI_AutoPolling() at stm32u5xx_hal_ospi.c:1,831 0x80042e8
ospi_memory_reset() at lx_stm32_ospi_driver_glue.c:560 0x8001afe
lx_stm32_ospi_lowlevel_init() at lx_stm32_ospi_driver_glue.c:79 0x800165a
lx_stm32_ospi_initialize() at lx_stm32_ospi_driver.c:61 0x80166ea
_lx_nor_flash_open() at lx_nor_flash_open.c:128 0x8015822
fx_stm32_levelx_nor_driver() at fx_stm32_levelx_nor_driver.c:111 0x8014758
_fx_media_format() at fx_media_format.c:177 0x8010a26
_fxe_media_format() at fxe_media_format.c:114 0x80144b8
fx_app_thread_entry() at app_filex.c:156 0x8001464
_tx_thread_shell_entry() at tx_thread_shell_entry.c:114 0x8018388
Other relevant info:
Board: MB1829 Discovery kit with STM32U5A9NJ MCU
Environment: STM32CubeIDE
Component: MX25UM51245GXDI00 Macronix OctaFlash
2023-09-02 5:57 AM
Perhaps a problem at the pin or peripheral level?
Would suggest finding some simpler OSPI examples, and debugging the BSP functionality, either confirming those work, or the specific issues with it.
2023-09-07 1:55 AM
Hello @efekete ,
Besides the @Tesla DeLorean proposal, I advise you to check the recommendation mentioned in Readme such as, for STM32CubeIDE add the following section into the .ld file:
._threadx_heap :
{
. = ALIGN(8);
__RAM_segment_used_end__ = .;
. = . + 64K;
. = ALIGN(8);
} >RAM_D1 AT> RAM_D1
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.