cancel
Showing results for 
Search instead for 
Did you mean: 

freeRTOS in STM32Cube_FW_H7_V1.6.0 on NUCLEO-H745ZI-Q

JLee.2254
Associate II

I am working on a project based on freeRTOS in STMCube_FW_H7_V1.6.0 and NUCLEO-H746ZI-Q.

When I compiles a CM7 code of the project, the port.c and the portmacro.h in ARM_CM4F (not in ARM_CM7) are used. (I am using MDK-ARM compiler 5.)

Are there no problems even if it use them?

In addition, when I compile it with ARM compiler 6, the codes related to freeRTOS gives many errors. How can I remedy them?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
TOlli
Senior

Hi,

I found this from the FreeRTOS forums:

https://forums.freertos.org/t/arm-cm7-instruction-set-present-arm-cm4f-core-which-leads-to-hard-fault-exception-reset-of-the-controller/8690

where it is said that those ports are the same.

And it would be helpful to see the output of the compiler, if you're looking for help in clearing the errors.

Best regards

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.