2022-11-16 8:58 AM
code generated for stm32l0xx with FAT option ticked, generates following stub, I believe missing the equal sign in if condition:
uint8_t FATFS_LinkDriverEx(const Diskio_drvTypeDef *drv, char *path, uint8_t lun)
{
uint8_t ret = 1;
uint8_t DiskNum = 0;
if(disk.nbr < _VOLUMES)
{
disk.is_initialized[disk.nbr] = 0;
disk.drv[disk.nbr] = drv;
disk.lun[disk.nbr] = lun;
DiskNum = disk.nbr++;
path[0] = DiskNum + '0';
path[1] = ':';
path[2] = '/';
path[3] = 0;
ret = 0;
}
return ret;
}
2022-11-16 9:09 AM
>> I believe missing the equal sign in if condition
No, C arrays indexes are ZERO based
/**
* @brief Global Disk IO Drivers structure definition
*/
typedef struct
{
uint8_t is_initialized[_VOLUMES];
const Diskio_drvTypeDef *drv[_VOLUMES];
uint8_t lun[_VOLUMES];
volatile uint8_t nbr;
}Disk_drvTypeDef;
2022-11-16 11:43 AM
exactly my point, when volume is equal 1 (you only have one volume) the 0 is not less than 0.
2022-11-16 12:23 PM
sorry my above comment is not right, there must be something else causing this function to be called two times, and only the second time the condition is not met, hence an error returned.
2022-11-16 12:33 PM
My fault, I was calling the function two times. Call to this function was already included in auto generated code in the FAT init.
void MX_FATFS_Init(void)
{
/*## FatFS: Link the USER driver ###########################*/
retUSER = FATFS_LinkDriver(&USER_Driver, USERPath);
/* USER CODE BEGIN Init */
/* additional user code for init */
/* USER CODE END Init */
}
2022-11-16 12:57 PM
Yes, it's not re-entrant, perhaps there are better ways of doing this, ST just did something very simple to meet their immediate needs, not necessarily production ready.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.