2017-11-23 8:17 AM
Hi,
I�m having some issues getting a dual FS USB Host RTOS configuration running based on a STM32F746 target.
Connection events and callbacks events work correctly.
When I use the USBH_Init() function for initialising USB FS1, the function is returning a valid Thread ID. The USB FS1 interface works like it should.
phost->thread = osThreadCreate (osThread(USBH_Thread), phost);
When I execute USBH_Init() a second time initialising USB FS2, the function is returning �0�. The USB FS2 interface doesn�t work.
Why is USBH_Init() returning a �0� thread when initialising USB FS2?
Thanks.
#usb2017-11-27 1:09 PM
Hi,
are there any specific RTOS changes/settings which need to be made in order to handle two FS USB Host interfaces?
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.