2018-02-06 11:41 PM
Hey,
I want to implement a �smart USB hub� (in software) which will include multiple devices, not a single compound device. Currently I can set the device address with the relevant register and get only the transactions relevant for that address, but I want to receive all transactions and then decide, in software, if I need to respond to it or not. My application may add or remove devices from this smart hub in runtime so a USB hub IC will not do.
Thanks in advance,
Assaf
#usb_device2018-02-07 5:43 AM
Does the STMF103 USB support a promiscuous mode?
AFAIK, no.
JW
2018-06-06 6:22 PM
Is promiscuous mode necessary for implementing a compound device (actually a hub)?
If so, do any other F0 or L0 chips have it?
Unfortunately, we'll need to make a similar thing soon :(
-- pa
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.