2025-03-26 10:46 PM
The problem ethernet link with NUCLEO-H755ZI-Q.
The conditions are as follows:
In this case, the Ack from the DHCP server could not be confirmed as being received.
dhcp->pcb_allocated is set to 0 (in function of dhcp_recv()).
A similar error has not occurred with CM7.
Do you happen to know the reason for this?
Solved! Go to Solution.
2025-03-28 12:47 AM
@MasatoKawatsuma wrote:
The above thread mentions MPU, but I don't use MPU in my environment.
・RTOS disabled
・MPU not used
No the problem in that thread is not only about the MPU configuration but also linked to the memory partition.
So check also your SRAM memory partitioning.
2025-03-27 12:30 AM
Hello @MasatoKawatsuma and welcome to the community,
Related question raised on this thread.
2025-03-27 9:25 AM
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Billy
2025-03-28 12:28 AM
The above thread mentions MPU, but I don't use MPU in my environment.
・RTOS disabled
・MPU not used
Also, the following warning occurred while debugging dhcp, so I think it might be a problem with pbuf memory management.
Assertion "pbuf_free: p->ref > 0" failed at line 753 in {path}/Middlewares/Third_Party/LwIP/src/core/pbuf.cIf you know anything, please let me know.
2025-03-28 12:47 AM
@MasatoKawatsuma wrote:
The above thread mentions MPU, but I don't use MPU in my environment.
・RTOS disabled
・MPU not used
No the problem in that thread is not only about the MPU configuration but also linked to the memory partition.
So check also your SRAM memory partitioning.
2025-03-28 1:58 AM
Thank you.
I had not assigned LWIP to SRAM3 in the linker file, so setting it as follows solved the problem.
MEMORY
{
FLASH (rx) : ORIGIN = 0x08100000, LENGTH = 1024K
RAM (xrw) : ORIGIN = 0x10000000, LENGTH = 256K
RAM_LWIP (xrw) : ORIGIN = 0x10000000 + 256K, LENGTH = 32K
}
...
.lwip_sec (NOLOAD) :
{
. = ABSOLUTE(0x10040000);
*(.RxDecripSection)
. = ABSOLUTE(0x10040060);
*(.TxDecripSection)
. = ABSOLUTE(0x10040200);
*(.Rx_PoolSection)
} >RAM_LWIP
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.