2019-06-11 8:55 AM
I'm looking for a eval board/micro-controller with high-speed USB (with integrated PHY) and I2S interface to stream up to 12 audio channels (6-in/6-out) 16-bit samples at 44Khz. Are there any app-notes or recommendations on audio over high-speed USB? Is this something that is supported in the Cube environment? Last I used it, it seemed to be limited to Full-speed USB.
Any suggestions? If not in Cube any suggestions on vendor-supplied stacks?
Thanks in advance,
2019-06-11 1:04 PM
> high-speed USB (with integrated PHY)
We can stop here, there's only one STM32 fulfilling this, the 'F723 (and it's crypto-enabled twin, if there is such).
JW
2019-06-11 2:35 PM
Hmmm... I'm guessing that's because of the "integrated PHY"?
Do things look better if I dropped that from the equation?
2019-06-12 12:27 AM
Well, the 'F723 has 2xSAI (each having 2 simplex channels) and 3xI2S simplex each, so that's 7 simplex channels whereas you require 12.
Depending on what exactly is the I2S device hung on, you might also use SPI, but in case of 'F723 that adds only 2 more. Maybe a H7 would have more.
I personally don't and wouldn't use Cube but have had a look and wasn't particularly impressed. Wrote my own USB umplementation, so can't recomment 3rd parties either. And I don't have experience with the OTG_HS in HS mode, so can't really comment e.g. on bandwidth, sorry.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.