2019-01-25 7:18 AM
We are writing a custom bootloader on STM32F102 and we
know we can write the flash memory in 16 bit wide steps.
We use now a continous binary flash image, so if it's length
would be odd we can concate one byte easily.
In near future we would like to use multi-region flash file
which contains section address and data length. Could it be
possible that the data lenght (in output sections) is odd? Do
the linker/compiler care of even data/section lenght? (For
example in read only data if it contains strings.)
2019-01-29 1:27 AM
I tried to put five bytes in a section, and the result:
FLASHX (rx) : ORIGIN = 0x800FC00, LENGTH = 1K
.myOutSection :
{
KEEP(*(.myOddSection*))
} > FLASHX
__attribute__((section(".myOddSection")))
uint8_t myArray[] = { 0xAA, 0xBB, 0xCC, 0xDD, 0xEE };
I use TrueSTUDIO and the GNU toolchain. I found these
bytes in the target flash area:
0x0800FC00
AA BB CC DD EE C2 20 03 FF FF FF FF ...
I read it during debug session through the Memory
Browser window. I saw three random bytes (the padding
bytes are different when I started a new debug session)
were put into the flash to round up the data to multiple
of four. I don't know how (linker/loader?) is responsible
for the rounding. Intristingly when i generate binary
image file, these padding bytes were not in the binary
file, only the AA BB CC DD EE bytes (these are the lastest
bytes of the file). So I tried to put padding bytes in a
controlled way:
__attribute__((section(".myOddSection")))
uint8_t myArray[] = { 0xAA, 0xBB, 0xCC, 0xDD, 0xEE };
__attribute__((section(".paddingSection")))
uint8_t paddingArray[] = { 0x11, 0x22, 0x33, 0x44 };
FLASHX (rx) : ORIGIN = 0x800FC00, LENGTH = 1K
.myOutSection :
{
KEEP(*(.myOddSection*))
. = ALIGN(4);
KEEP(*(.paddingSection*))
} > FLASHX
0x0800FC00
AA BB CC DD EE 00 00 00 11 22 33 44 00 00 00 00 FF FF FF FF ...
I get unexpectedly four zeros after the 44, but the generated
binary file length (and the length of myOutSection) is multple
of four.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.