2021-10-07 10:38 AM
Hi
I cannot understand why my opt.h file cannot see the lwipopts.h file in the same folder.
Presumably, it must be something to do with the 'Wno-stringop-overflow' warning.
This contains a very long string -
-mcpu=cortex-m7 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DSTM32H743xxDUSE_STM32H7XX_NUCLEO_144_MB1364 -c -I../../../Src -I"D:/halfcontainer/projects/cubeideN/LwIP_HTTP_Server_Netconn_RTOS/SW4STM32/STM32H743ZI_Nucleo/Middlewares/LwIP" -I../../../Drivers.......+ about 200 chars-
Can anyone tell me how to find out whats happening?
Trying to look back at sys_arch.c is a bit frightening! (To me at least)
Thanks,
Chris
18:12:19 **** Incremental Build of configuration Debug for project LwIP_HTTP_Server_Netconn_RTOS ****
make all
arm-none-eabi-gcc -Wno-stringop-overflow "../Middlewares/Third_Party/LwIP/system/OS/sys_arch.c" -mcpu=cortex-m7 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DSTM32H743xx -DUSE_STM32H7XX_NUCLEO_144_MB1364 -c -I../../../Src -I"D:/halfcontainer/projects/cubeideN/LwIP_HTTP_Server_Netconn_RTOS/SW4STM32/STM32H743ZI_Nucleo/Middlewares/LwIP" -I../../../Drivers/CMSIS/Device/ST/STM32H7xx/Include -I../../../Drivers/STM32H7xx_HAL_Driver/Inc -I../../../Drivers/BSP/STM32H7xx_Nucleo -I../../../Drivers/BSP/Components/Common -I../../../Drivers/BSP/Components -I../../../Middlewares/Third_Party/LwIP/src/include -I../../../Middlewares/Third_Party/LwIP/system -I../../../Middlewares/Third_Party/FreeRTOS/Source/portable/GCC/ARM_CM4F -I../../../Middlewares/Third_Party/FreeRTOS/Source -I../../../Middlewares/Third_Party/FreeRTOS/Source/CMSIS_RTOS -I../../../Middlewares/Third_Party/FreeRTOS/Source/include -I../../../Utilities -I../../../Drivers/CMSIS/Include -Os -ffunction-sections -Wall -fstack-usage -MMD -MP -MF"Middlewares/Third_Party/LwIP/system/OS/sys_arch.d" -MT"Middlewares/Third_Party/LwIP/system/OS/sys_arch.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Middlewares/Third_Party/LwIP/system/OS/sys_arch.o"
In file included from ../../../Middlewares/Third_Party/LwIP/src/include/lwip/debug.h:41,
from ../Middlewares/Third_Party/LwIP/system/OS/sys_arch.c:34:
../../../Middlewares/Third_Party/LwIP/src/include/lwip/opt.h:51:10: fatal error: lwipopts.h: No such file or directory
51 | #include "lwipopts.h"
| ^~~~~~~~~~~~
compilation terminated.
make: *** [Middlewares/Third_Party/LwIP/system/OS/subdir.mk:19: Middlewares/Third_Party/LwIP/system/OS/sys_arch.o] Error 1
"make all" terminated with exit code 2. Build might be incomplete.
18:12:25 Build Failed. 2 errors, 0 warnings. (took 5s.573ms)
Solved! Go to Solution.
2021-10-26 3:33 AM
Hello @clock.1166 ,
Go to Project options ->C/C++ tab->Include paths and add new paths to your include directories.
I advise you to review this FAQ: How to create project for STM32H7 with Ethernet and LwIP stack working.
When your question is answered, please close this topic by choosing Select as Best.
If you still have issues, don't hesitate to come back to the Community.
Imen
2021-10-26 3:33 AM
Hello @clock.1166 ,
Go to Project options ->C/C++ tab->Include paths and add new paths to your include directories.
I advise you to review this FAQ: How to create project for STM32H7 with Ethernet and LwIP stack working.
When your question is answered, please close this topic by choosing Select as Best.
If you still have issues, don't hesitate to come back to the Community.
Imen
2021-11-01 2:03 AM
Hi @clock.1166 ,
Were you able to resolve the issue you described here?
If yes, it will be interesting to share with us the solution you found and marked the best answer to close this post.
Imen
2021-11-01 2:21 AM
2021-11-17 5:18 AM
Yes Thanks. That did the problem!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.