2021-12-10 8:39 AM
MCU: STM32F030RC
CubeMX Firmware Package: STM32Cube FW_F0 V1.11.3
Actual code snippet from stm32f0xx_hal_uart.h:
/** @brief Flush the UART Data registers.
* @param __HANDLE__ specifies the UART Handle.
* @retval None
*/
#define __HAL_UART_FLUSH_DRREGISTER(__HANDLE__) \
do{ \
SET_BIT((__HANDLE__)->Instance->RQR, UART_RXDATA_FLUSH_REQUEST); \
SET_BIT((__HANDLE__)->Instance->RQR, UART_TXDATA_FLUSH_REQUEST); \
} while(0U)Compiler error:
Drivers/STM32F0xx_HAL_Driver/Inc/stm32f0xx_hal_uart.h:500:45: error: 'USART_RQR_TXFRQ' undeclared (first use in this function); did you mean 'USART_RQR_RXFRQ'?
2021-12-10 1:53 PM
Officially, in 'F030, USART_RQR.TXFRQ does not exist, see RM0360. The reason is, that it's bound to Smartcard mode, which is officially not implemented in the 'F030. Thus, this is formally a CubeFW error.
JW
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.