2021-12-16 11:23 PM
Hi,
I am working with STM32F429ZI. Project consists of TFTP , TCP/IP , Flash and Free RTOS. I have got this error and not able to solve. Please provide solution if anyone facing the same.
Thanks
Anagha
Solved! Go to Solution.
2021-12-17 7:08 AM
Probably there is an out of bounds array write or a stack overflow condition. It could be other things, but those seem the most likely.
2021-12-17 5:39 AM
There is no memory at 0x3100272c, so the error, you need to find out what causes this bad pointer. Compile with a recent compiler and high warning level and carefully check the warning. So possible uninitialized variable can be the cause, as many other things
2021-12-17 7:08 AM
Probably there is an out of bounds array write or a stack overflow condition. It could be other things, but those seem the most likely.
2021-12-27 4:03 AM
Hi,
Thanks Uwe Bonnes and TDK.
I got solution over this problem. Actually I had defined the 10K area in linker file using attribute. But forget to initialize it with zero. so the problem is occured of memory overlapping and no debug information available. But initialization with zero to that area working successfully.
Thanks
Anagha Dankh
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.