STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

We wanna make use of IEEE 1588 (PTP), but I am not sure what is the use Ethernet PTP target time high and low registers. And how is it used to get the PTP trigger output

For PTP implementation in STM32F427 we have decided to use PTPd stack but I am not able to understand what is the use of Ethernet PTP target time high and low registers in achieving time synchronization.

KMark.1 by Associate II
  • 877 Views
  • 0 replies
  • 0 kudos

USB bootloader for STM32F103CBT6 for ST-Link design

We' re planning to implement ST-Link (USB to SWDIO) HW design using STM32F103CBT6 microcontroller. This HW design is similar to any STM32 Nucleo board's ST-link HW design.  What I understood is STM32 controller will be having default UART bootloader ...

S.Kamath by Associate III
  • 1229 Views
  • 0 replies
  • 0 kudos

STM32F107 RNDIS

Hello guys,We have an RNDIS code that we use with STM32F070. We are trying to adapt this code to STM32F107. However, we could not find the equivalent of the code snippet below in STM32F107. Could you help? (We are using Cubemx.) #define RNDIS_CONTROL...

gmut.1 by Associate
  • 713 Views
  • 0 replies
  • 0 kudos

Method for STM32L4R9ZIJ6 change boot mode?

I have one STM32L4R9ZIJ6, and I loaded BootLoader on 0x08000000 and BLE Sensor bin on 0x8005000. However, when the board doesn't seems boot into the program. Red LED flashing when plugged USB power. Using Flash Loader, it ask for verify boot mode con...

YYu.2 by Associate III
  • 706 Views
  • 0 replies
  • 0 kudos

Resolved! Bootloader troubleshooting

Hello. I'm using an STM32F3, and am struggling to get the bootloader working on my custom board. It works on the F3 discovery board (If you remove SB19 and wire up a pull-high).Steps: Plug USB port into PC. Boot1 is confirmed to be set high in MCU so...

DOCon.1 by Senior
  • 3393 Views
  • 3 replies
  • 0 kudos

USB Serial communication on STM32L562E-DK

Hello,I want to send and receive data between my STM32L562E-DK Discovery Board and my pc via USB.The best way would be to use the Micro-USB port which also feeds the ST LINK (CN17). Is there an easy way to implement serial receive and send functions?...

MPetr.3 by Associate III
  • 648 Views
  • 0 replies
  • 0 kudos

[STUSB4500 <--> STM32L031K6] Is it possible to parallelly access read/write register through I2C and NVM register through GUI without any affect?

We are currently working on a USB type C based fast charging system design and interfacing STUSB4500 with STM32L031K6 to compliant PD for fast charging. We are successfully able to read and write registers through I2C.So Is it possible to parallelly ...

Bhautik by Associate II
  • 944 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.