STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

RTOS is not working in STM32F072.

I have created a project in STM32CubeIDE with UART and some GPIO's as Input and Output.I have created 2 Tasks using FreeRTOS - CMSIS v1(osPriorityNormal, osPriorityBelowNormal) with different osDelay(osDelay(500);, osDelay(600);). I have compiled and...

AP.6 by Associate
  • 1283 Views
  • 1 replies
  • 1 kudos

STA8090WG CAN and USB

Hello,We are interesting STA8090WG as they support both CAN and GPS.However, after simply review with data sheet, I have some questionsIs it right ? Once we use CAN, we can't use USB since those are alternated with same pin.Can we get reference schem...

HKwon.2 by Associate
  • 614 Views
  • 0 replies
  • 0 kudos

Bad init in LL for systick.

I try use systick handler in STM32G0 uC, i use LL libray. In funcion to activate Systick ( void LL_InitTick(uint32_t HCLKFrequency, uint32_t Ticks) ) is a bug.The error consists in incorrect setting of the SysTick-> CTRL (STK_CSR) configuration regis...

PKuni.1 by Associate
  • 1090 Views
  • 1 replies
  • 0 kudos

Can we use ST VID and PID in commercial product?

We are trying to build a usb temperature logger. As we know that while using usb cdc we have to define VID and PID to the usb middleware. I have some question:1.Can I use ST's VID and PID in our final product version?2.If so, can I redistribute ST's ...

JKSah by Associate II
  • 2592 Views
  • 3 replies
  • 0 kudos

I2C - I want to read data from the register by the HAL (HAL_I2C_Mem_Read) but 8 bit every rime is LOW but should be HIGH.

Hello everybody!!)) I spent a few days already, try to decide this problem, this reason I decided to ask here.I can write data to register by command HAL_I2C_Mem_Write, but can not read, because 8 register is low uint8_t adress_read1 = 0x43; uint8_t ...

0693W000006GZQKQA4.jpg
IRakh.1 by Associate III
  • 4426 Views
  • 7 replies
  • 0 kudos

STM32H742IIT6: Using both USB ports as HID hosts?

Has anyone any experience of using both USB ports on a H7 as HID hosts? Use is for a mouse and keyboard. Does the ST USB host firmware support using both ports in this way?I can start work on this but it would be nice to know ahead of time that it h...

PMath.4 by Senior III
  • 1231 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.