STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Bootloader programming using UART with STlink V2.1

Hello guys,I have a small question I have st link v2.1 which comes with the Nucleo board, so I need to program another custom board using this st link, but I have to do using UART (Rx, Tx) pins which is nearby the SWD connector, please if anyone has ...

Roshan by Associate III
  • 3379 Views
  • 3 replies
  • 0 kudos

OBL_LAUNCH with Bootloader (ST ROM) in STM32L0

Hi,I have STM32F030 which is connected to STM32L082 with UART (Rx/Tx), RESET and BOOT0 line. When needed STM32F030 is able to restart STM32L082, run ROM Bootloader, erase and program flash.But when I have clean STM32L082, empty flash on it on product...

qbaj by Associate II
  • 1065 Views
  • 0 replies
  • 0 kudos

ST25R3916-EMVCO UART1 Configuration. I can not configure the UART1 (pins PA11, PA12) to communicate through the USB.

I have seen a similar thread for the ST25R3916-DISCO (making appropiate changes in stm32l4xx_hal_msp.c ), however in this board the USB pins are not connected to the same pins and I am not capable of correctly reconnect the solution to PA11, PA12.UAR...

PablodMM by Associate II
  • 837 Views
  • 0 replies
  • 0 kudos

Resolved! USB SUPPORT

@Ons KOOLI​. ​Hi, i want to use stm32f103 or stm32f1 family microcontroller for mass storage in usb for data logging.any reference and example are pretty useful as i am new to usb logging with stm32.​

ABhat.7 by Associate III
  • 10007 Views
  • 20 replies
  • 0 kudos

Resolved! Understanding HRTIM fault filter lengths

HiI am trying to implement a fault filter for the HRTIM on a stm32G474.I am using the LL libraries and the Reference manual.I find the table 234 in the reference manual completely unreadable and confusing. Could someone please explain how it is suppo...

marbel by Associate II
  • 1959 Views
  • 2 replies
  • 0 kudos

STM32H743 USB Host MSC maximum throughput

Hi everybody,I am using stm32h743i-eval2 and I need to write data on an USB stick via USB HS.It configured by Stm32Cube easly and I could write data as well. But I don't know why the device is too slow. Throughput is about 1.2MBps via HS USB.Is that ...

ataro.1 by Associate
  • 1515 Views
  • 1 replies
  • 0 kudos

HardFault is occurred when I use DSP with FreeRTOS

I am trying to run DSP Functions like as FFT with freeRTOS which use multiple tasks.And HardFault is occurred from prvPortStartFirstTask() for calling FFT functions.So I don't have any idea what i check.. Please help me which parts I will check.. Tha...

YHong.2 by Associate
  • 1468 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.