STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FreeRTOS and timebase interrupt priority

I’m using STM32Cube MX 6.2.1, STM32Cube IDE 1.6.1 and STM32Cube_FW_H7_V1.9.0 for a STM32H7A3 project. As recommended, I configured the HAL time base source to a timer other than systick. (TIM17) If I understand correctly, FreeRTOS uses systick and se...

AMacI.1 by Associate II
  • 2573 Views
  • 1 replies
  • 0 kudos

STM32H743 Ethernet: can ETH access SRAM4?

Hello, I am writing a driver for the Ethernet interface, and I noticed it fails to read data from buffers lying in SRAM4 (0x38000000 - 0x3800FFFF), with a Fatal Bus Error. According to the MCU's Reference Manual (RM0433) 2.1 Table 3, and 2.1.6 Ethern...

LDroz.2 by Associate II
  • 2045 Views
  • 2 replies
  • 0 kudos

Resolved! Where is the firmware for the STM32F411E-DISCOVERY board???????? In one of the user manuals, it was mentioned that there is a single zip file with demonstrations, examples etc for MDK-ARM, EWARM and something else.

But I am having a hard time finding this zip file!!!!! I want to start using my stm32f411e discovery board but there are hardly any resources on the internet for this specific board and for a newbie like me this is just demotivating. Please help me o...

KP.3 by Associate II
  • 2052 Views
  • 2 replies
  • 0 kudos

Resolved! STL versioning

We are integrating the STL library in the context of a project requiring IEC 61508 safety integrity level 2 (SIL2). How can we programmatically pull the version info out of the STL library? The API doesn't show anything to that effect. Also, what's t...

DamienF by Associate II
  • 2043 Views
  • 2 replies
  • 0 kudos

Ethernet TcpEchoServer

The issue am facing is . I have created 4 maximum connection for 1 port at particular 1 ip. When i open port of same port number and same IP on terminal the data travel should travel to both the ports. But it comes on only single port.tcp_write(Perso...

Divyanshu by Associate II
  • 1084 Views
  • 1 replies
  • 0 kudos

Second buffer in ethernet DMA is not transmitted

Hi, I'm using STM32H7 nucleo board and I have written a simple UDP client that receives a message and loops it back. I was using the LwIP Socket API for this (lwip_sendto) and using Wireshark I can see that packets are coming out of the board, but th...

IKayk.1 by Associate II
  • 1218 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.