STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ISSUE with STSAFE_Provisioning project in X-cube_AWS

hi i am trying to run AWS_DEMOS project on b-l4s5i-iot01 board. i build stsafe_provisioning project but got the error mentioned below after the programming the image.i could use some help. build doesn't throw any errors. and i haven't changed anythin...

NKuma.9 by Associate II
  • 1558 Views
  • 1 replies
  • 0 kudos

CMSIS-DSP DC offset problem [Solved]

Hi everyone,I am developing a sound acquisition node with MEMS-Microphone and everything works fine except that the FFT output not as it's supposed to be! even it's work and frequencies in the input data is detected good but imag[0] != 0 why? and it ...

0693W000005BorMQAS.png 0693W000005BorgQAC.png 0693W000005BoqtQAC.png

STM32H7 firmware updgrade using ethernet

Hello!I am currently working on a project using the stm32h74.In previous projects i have used this mechanism using UART or SPI but never ethernet.Trying to understand wether it is possible to use the built in stm32 bootloader using ethernet?Thanks :)

yuri CH by Senior
  • 3468 Views
  • 4 replies
  • 0 kudos

Resolved! STM32H7 USB Full Speed SOF interrupt. I used the CDC class as a template to implement a cusom vendor class. It seems to me that the Start of Frame interrupt never fires. How do I enable it?

I am attempting to send data in bulk, 64 bytes at a time for every SOF interrupt, however I don't see how to enable the interrupt.I attempted defining USE_HAL_PCD_REGISTER_CALLBACKS as 1, but that doesn't seem to trigger the SOF interrupt.

NBaro.1 by Associate II
  • 2016 Views
  • 1 replies
  • 1 kudos

I cannot use USB DFU bootloader

I am using STM32L082KZT6 and want to use bootloader with USB. I have read instruction and in my perspective I thought that just by connecting boot0 pint to high then usb bootloader mode would start. But it didn't. I putted the schematic picture belo...

0693W00000D0xMdQAJ.png
SShir.2 by Associate II
  • 1835 Views
  • 3 replies
  • 0 kudos

I have a lot of questions about USBX

How does the FIFO created in MX_USB_Device_Init() match the endpoint?In the USBX document of Azure, the descriptor is directly made into an array, while the sample program uses a lot of functions to implement it. What are the benefits of this? Not ea...

arilink by Associate III
  • 1153 Views
  • 1 replies
  • 0 kudos

Resolved! Why does FatFS work sometimes, and sometimes not?

Hi!I'm using FatFS R0.11 with STM32F373 and sometimes it works to use FATFS and sometimes not.These are the issues I got and I don't know why. Can it be something with NVIC interrupts that causing issues with the FatFS library?Mount SD card: Mount SD...

0693W00000D0tRxQAJ.png 0693W00000D0tFIQAZ.png
DMårt by Lead
  • 3980 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.