STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

About library of built-in bootloader

Hi,There are host and slave MCU, both are ST MCU. Slave MCU does not have wifi/ble for OTA upgrade. I would like to use host MCU to download slave MCU image and then use built-in bootloader to upgrade slave MCU.I can find the communication protocol d...

John_1992 by Associate II
  • 1555 Views
  • 2 replies
  • 0 kudos

STM32F103 uwTickPrio error in debug mode

Hi! I'm using STM32F103C8 as MCU. I am quite new to st environment and trying to warm up to cubeide interface & HAL libraries. I am going to design quite complicated circuitry and it requires many pins but the ideal one i picked is F103C8 since i hav...

0693W00000DmwwpQAB.png

STM32F7508-DK not supporting the audio input?

Hi,I'm wondering why the STM32CubeF7 1.16.1 package only supports "microphone 2" (INPUT_DEVICE_DIGITAL_MICROPHONE_2) within stm32f7508_discovery_audio.c / BSP_AUDIO_IN_OUT_Init() ?Is there a technical reason to do so?I would like to record audio thro...

gflix by Associate II
  • 1246 Views
  • 1 replies
  • 0 kudos

Resolved! NUCLEO-L4R5ZI Changing timebase source fails

Hello,STM32Cube FW_L4 V1.17.0When changing the timebase of the systick, the HAL_Init() function no longer returns and it goes off to system memory in a loop.To replicate, start a new project with for the NUCLEO-L4R5ZI, initialise all pins to the defa...

DM.7 by Associate III
  • 1550 Views
  • 2 replies
  • 0 kudos

Resolved! Default bootloader source code?

My dedicated hardware does not support uart/i2c/spi on the pins that are mentioned in AN2606. To update firmware IAP, I need to write my own bootloader that behaves the same as the default one (I want to use stm32flash tool as host, which fasten my w...

BMich.2 by Associate
  • 1543 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.