STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BL475E-IOTA library fails while sending data

BL475E-IOTA library fails while sending data to the MQTT broker. I see the below prints on the console. I'm using the default STM32 library for AWS. Can anyone please let me know why I'm seeing these errors. Thank you.STM32CubeExpansion_Cloud_AWS_V1....

PTeja.1 by Associate
  • 1693 Views
  • 2 replies
  • 0 kudos

Config.h

Can someone give me a config.h file for the H735 Discovery kit ?Cannot get past the compile errors...There is nothing in my config file

T J by Lead
  • 1741 Views
  • 2 replies
  • 0 kudos

Resolved! Regarding of stm32f070c6t6 boot loader.

Hello,I am working on the stm32f070c6t6 controller, i just want to use this controller at replacement of Arduino. Arduino has the boot loader code, on that we will write our regular code as function specific code. same thing i want to do this by usin...

RKUMA.2 by Associate II
  • 1631 Views
  • 2 replies
  • 0 kudos

RTOS f_mount() Heap Leak in HEAP_1 model

I have a 1 second loop that tries to mount the SD card, It repeatedly calls f_mount() until an SD is detected, however, I've noticed that there is a semaphore created each time f_mount() is called which is not deleted in HEAP_1 mode. So after some ti...

ETH hardware present but no software, safe?

We have the below ETH pins connected to a KSZ8081RNACA-T with the pins setup in alternate function for ETH, there is no code for initialization of ETH as of now (future implementation). We have had a few processors die with 3.3v shorting to gnd, coul...

PCudd by Associate II
  • 1334 Views
  • 1 replies
  • 0 kudos

DRP1M1 with NUCLEO-G0B1RE

Hello to All,When looking into the datasheet of the DRP1M1 addon for USB-PD, it was mentioned that this board could be used together with the NUCLEO-G0B1RE.However.The TCPP_V3.0.0 does not contain sources for this nucleo board !Are they available som...

Alfredo by Associate II
  • 9324 Views
  • 11 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.