STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F429I Read file data via USB

Hello everyone,Very new to STM family.I'm trying to read data via FRESULT Read_File (char *name) function.I've copied data from CubeProgrammer from specific sector and saved it in USB and want to read and upload that data via USB.Can anyone shows me ...

Ofaro.1 by Associate II
  • 809 Views
  • 0 replies
  • 0 kudos

STM32H747 USB audio DataOut issue

Hi together,I'm trying to make a basic USB audio speaker from STM32H747 DISCO board with Cortex-M7.I start a new CubeMX project for this board, add in the USB_HS and audio drivers on default settings.Once I do this, the Windows 10 machine will see th...

0693W00000JOnfWQAT.png
JCheng by Associate
  • 1803 Views
  • 1 replies
  • 0 kudos

Resolved! How can I program and / or debug the microcontroller of a NUCLEO-H743ZI2 without the CN1 micro USB connector?

Hello Community,I have a curiosity to ask you. I have a NUCLEO-H743ZI2 without its micro USB connector (STLINK-V3E USB connector CN1).I would like to know if it was possible to continue programming and debugging on the microcontroller integrated into...

0693W00000JPzSqQAL.png
VNava.1 by Associate III
  • 3694 Views
  • 4 replies
  • 0 kudos

STM32F103 bootloader issue

Hi all.I am using the STM32F103RBT6 microcontroller.Some MCUs mounted on the board did not run the bootloader.When I checked system memory ​address(0x1FFFF000 - 0x1FFFF800) with STM32CUBEIDE , The range of the address is filled with 0xff(attached fi...

Tsugi.1 by Associate II
  • 6990 Views
  • 5 replies
  • 0 kudos

Resolved! We are trying to to read and write to a SD card. We are using the STM32F50N8. Find below attached the schematic for the SD card and the GPIO. We have set it up the same we as mentioned here (SD 4 bit wide mode) - https://www.youtube.com/watch?v=

Hi, We are trying to to read and write to a SD card. We are using the STM32F50N8. Find below attached the schematic for the SD card and the GPIO. We have set it up the same we as mentioned here (SD 4 bit wide mode) - https://www.youtube.com/watch?v=I...

0693W00000JPK4OQAX.png 0693W00000JPK4JQAX.png
PMold.1 by Associate III
  • 1998 Views
  • 3 replies
  • 0 kudos

Importing project errors

Hello everyone, I am trying to clone a project from https://github.com/SEDSIIT/nova-flight-computer, and whenever I try to import it in the Cube IDE there are errors with the project, both when I get it from GitHub and from a zip from the original au...

Caitlin by Associate
  • 1183 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.