STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32 NetX Duo LwM2M Firmware Update

I have a project with STM32 MCU and BG95 LTE module. I use NetX Duo with LwM2M protocol. I am trying to implement FOTA for STM32 with LwM2M protocol. I haven't find resources for that. Is there any example for that?How can I implement that function? ...

MKILI.3 by Associate
  • 1472 Views
  • 1 replies
  • 0 kudos

Receive UDP broadcast from a particular source port

Hi all,I am working on a project that transmits UDP packet to a remote IP and port. I need to receive a broadcast packet from a particular source port. Below is my current UDP initialization.I am using LWIP stack for UDP communication. How should I i...

SSala.3 by Associate III
  • 1374 Views
  • 0 replies
  • 0 kudos

Resolved! How to use STM32 as a USB host and mount USB device??

/* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "usb_host.h" #include "usbh_core.h" #include "usbh_msc.h" /* USER CODE BEGIN Includes */ #include "ff.h" /* USER CODE END Inclu...

jsoda.1 by Associate III
  • 3942 Views
  • 2 replies
  • 0 kudos

Hello guys, I am working with STM32G0C1RET6. I want to use STM32 as a USB host and want to save data on USB flash stick. I followed some tutorial from ST microcontroller's youtube channel but I am still not able to mount my USB device. what should I do?

Here are details about my project:I have connected my USB_DM and USB_DP pin directly to USB connector.I enable A9 and selected as a GPIO output using VBUS setting in CUBEIDE. Which is providing me 3.3VI read that there is inbuilt pull up resistor in ...

jsoda.1 by Associate III
  • 4257 Views
  • 12 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.