STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-STL library for STM32U5

Hi, we're transitioning our platform from a STM32F412 to a STM32U575, and in our project we are currently using the X-CUBE-STL libraries to perform runtime safety monitoring functions.It seems that the package does not yet support the STM32U5 family....

SBone.3 by Associate II
  • 2192 Views
  • 1 replies
  • 0 kudos

Trying to run Azure IoT Central Quick Connect Script on B-U585I-IOT02A But getting the following error: Device ID contains invalid characters.

Trying to run Azure Iot Central Quick Connect Script on B-U585I-IOT02A1.Downloaded x-cube-azure software package fromwww.st.com/en/embedded-software/x-cube-azure.html2.Then navigated throughproject\en.x-cube-azure_v2-0-0\STM32CubeExpansion_Cloud_AZUR...

0693W00000QLLEAQA5.png 0693W00000QLLFNQA5.png
YAgar.11 by Associate
  • 2114 Views
  • 3 replies
  • 0 kudos

Define the Option Bytes in the code

Hello, I am new user and I am using SMT32G031K8.I am finalizing the development of my code and I have one last problem with the "OPTION BYTE"Topic: I need to change the IWDG_STOP bit of the USER configuration OptionByteTest carried out: I have succes...

DCall.2 by Associate
  • 2428 Views
  • 2 replies
  • 0 kudos

STM32f7 USB Host controlling 4G Modem

Posted on December 18, 2017 at 15:55I'm trying to link my stm32f7 to a Telit LE910 modem over USB. I can already do this over a UART but I want to increase the data rate.My hope is to use the stm32 USB Host CDC drivers.I can enumerate the device and...

Danish1 by Lead III
  • 12747 Views
  • 22 replies
  • 0 kudos

RNDIS(TCP/IP over USB) for STM32H7B3IIK6Q

Hello,I want to know whether STM32H7B3IIK6Q can be configured as an USB communications class RNDIS devices, so it can communicate with an network device, it is TCP/IP over USB.If it support, how can I get start with my design, is there any applicatio...

WLiao.1 by Associate II
  • 3553 Views
  • 2 replies
  • 0 kudos

Resolved! Unable to activate UCPD Trace in STM32G431

Hi,​ I have tried many times to get a trace using STM32CubeMonitor-UCPD 1.2.0 with my board without success. I have tried with both RTOS and without. The USAR1 is connected to an FTDI usb serial cable but the board doesn't show up In the monitor....

Correa by Associate II
  • 6475 Views
  • 8 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.