STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

HAL_DMA_XFER_CPLT_CB_ID not firing - STM32H7

Looking at this post pwm and callbacksIt does indeed look like the PWM pulse callback is used rather than the HAL_DMA_XFER_CPLT_CB_ID CalllbackI have set up DMA to transfer to PWM. It is a circular buffer so I am just changing the pointer "audio_chan...

I am designing a board with STM32 device of P/N STM32G4A1KEUx. I am trying to see if I need to have an external pull up on the USB-FS D+ line for detection. The usual application note don't seem to include this device as it looks.

I am designing a board with STM32 device of P/N STM32G4A1KEUx. I am trying to see if I need to have an external pull up on the USB-FS D+ line for detection. The usual application note don't seem to include this device as it looks. Does this device ha...

BPart.1 by Associate II
  • 1507 Views
  • 3 replies
  • 0 kudos

Resolved! What is the correct Vector Table base offset in HAL library STM32Cube FW_H7 V1.10.0 (STM32H730VB)?

I have two projects:  ·                both on microcontroller STM32H730VB; ·                both created in STM32CubeIDE Version: 1.10.1 with HAL library STM32Cube FW_H7 V1.10.0; ·                HAL version in file stm32h7xx_hal.c: STM32H7xx HAL D...

DWiśn.1 by Associate II
  • 3587 Views
  • 4 replies
  • 0 kudos

Ethernet not performing hardware CRC on STM32F765

I'm bringing up an Ethernet project with the latest FreeRTOS+TCP and SPL ported from the F407.I've got it sending packets but the responses to the ICMP when I ping the device come across in wireshark as having invalid CRCs of all zeros (see wireshark...

0693W00000GWq4NQAT.png 0693W00000GWq4DQAT.png
LMore.5 by Associate II
  • 3073 Views
  • 7 replies
  • 0 kudos

Resolved! STM32L4 SPI SD Card with FATfs and USB MSC

Hi all, I am working on a custom data logging board using STM32L4 and an SD NAND (uSD card in form of an IC). Since the SD chip is a surface-mounted IC (https://www.adafruit.com/product/4899) on the board using SPI and FATfs so I want to implement US...

PLy.1 by Associate II
  • 8174 Views
  • 7 replies
  • 0 kudos

Resolved! Modify usbd_stoge_if.c to use SD Card trougth SPI

Hi to all,I managed to interface with the SD card through the SPI and the FaTFS library (thanks to https://01001000.xyz/2020-08-09-Tutorial-STM32CubeIDE-SD-card/) now I need to implement a USB mass storage device on the same hardware.i don't know how...

ABatt.1 by Senior
  • 5143 Views
  • 5 replies
  • 1 kudos

Stm32 USB OTG Host and Device

Hello everyone,I have recently started working with a Nucleo board based on STM32L4R5. IDE: STM32CubeIDE and the HAL drivers.I am trying to use the USB on the Nucleo board as OTG(both Host and Device depending on the connection). I am not found any e...

POval.1 by Associate II
  • 4705 Views
  • 3 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.