STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Timer and uart does not work at the same stime

Hello,In my code there are custom bootloader part and user application part. I init watchdog timer and refresh watchdog timer in the bootloader part and user app part. The code goes to user app from bootloader by jumping address. Likewise, The code g...

MTapu.1 by Associate II
  • 3026 Views
  • 5 replies
  • 0 kudos

STM32F103 FW standalone upgrade is possible?

Hi guys, some body make it a standalone upgrade for this small MCU ¿? This MCU can use the native USB in OTG FS mode with a correct bootloader i think can do it, if somebody with more experience can clarify this please.Thanks

woutnme by Associate II
  • 1611 Views
  • 1 replies
  • 0 kudos

Hi, Want to know if a STM32H7A3Z1-Q can configure as USB OTG Host ? We tired the configuration as per online tutorials and the device is not entering into HOST_USER_CLASS_ACTIVE state.

The other end of USB is a custom board which can act as a CDC device.(When connecting the custom board to PC, interface showing as per the attachment.. Showing as RNDIS interface and 3 virtual COM Port.)Attached code which we tried for USB host. Pl...

JJoy.1 by Associate III
  • 1169 Views
  • 0 replies
  • 0 kudos

Ethernet is not detecting after assigning the Static IP

Greetings !I am using Azure RTOS on STM32H743 and I tried setting up the Static IP for Ethernet. I could successfully able to assign Static IP . Here after this I am observing that , most of the times IP address is assigning only when I remove and r...

PG.9 by Associate III
  • 1719 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.