STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Does the latest version of the driver of STM32H735VGH6 supporting USB audio and HID composite device functionality?

I want to use the USB interface of STM32H735VGH6 to develop the functions of USB audio and HID composite devices.I have a question, is the latest version of the driver supporting USB audio and HID composite device functionality? If supported,please l...

jding.11 by Associate II
  • 1857 Views
  • 1 replies
  • 1 kudos

I have stm32f413vht6 board and i want to send data to aws iot using mqtt protocol for internet we want to use mc60 gsm module can it be possible and if possible then provide some example or guide me .

I have learn something from internet they are saying use aws iot sdk for embedded c . let me know in this library how to copy in keil vision my project and how to add certificate details we can add of our aws iot credential into this library. help m...

GMish.2 by Associate
  • 895 Views
  • 0 replies
  • 0 kudos

Resolved! Composite device on stm32f4

Hi! I am trying to implement a composite device (two VCPs) on my stm3f4 board, as I need to transmit data simultaneously to the pc. I see that I have enough endpoints to do so but have no idea where to start from. Do you have any clear examples pleas...

LOnGr.1 by Associate III
  • 2324 Views
  • 1 replies
  • 0 kudos

Error when configuring STM32H5 clock tree.

Using STM32CubeMX v6.8.1. Target is STM32H573. Syntax error in "Clock Configuration":Initializing: STM32H573RITx LogicalParser: syntax error detected in expression for RCC original expression: ((VCOInputFreq_Value >1000000|(VCOInputFreq_Value=100000...

koendv by Associate III
  • 1622 Views
  • 1 replies
  • 0 kudos

Using STM32F4 with wireless mouse

Hi,Defining a host of an HID wired mouse, on an stm32f4 MCU works great.Trying to use a wireless mouse doesn't work at all.The wireless mouse comes in a pair with a keyboard. Pressing a button on the wireless keyboard works well but clicking/moving t...

ZIgon.1 by Associate II
  • 1483 Views
  • 1 replies
  • 0 kudos

NUCLEO-H723ZG using Ethernet/Ping Problem

Hello,I got the NUCLEO-H723ZG board to save ADC data fast enough. I don't have any experience with ETH. So I wanted to begin simply. I tried to use some tutorials and examples but the board doesn't respond to pings.I tried:1- The "LwIP_UDP_Echo_Serve...

ADynr.1 by Associate II
  • 4023 Views
  • 4 replies
  • 0 kudos

Difference between STM32CubeIDE and GDB

I'm a newbie to STM32 programming, but have 25+ years in desktop development.I've created a PCB with a STM32F042F6 mcu (based on a working design). I added pins for a SWD port and I have an LED connected to PortB1.I've used STM32CudeIDE to create a s...

DMoor.6 by Associate II
  • 1824 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.