STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB Host mode in STM32F429ZI nucleo board

Hi I'm using STM32F429ZI Nucleo board to work on integrating C270 Logitech camera through USB host. I'm not getting any interrupt in the USB IRQ handler when the device is connected. And it is said that LD8 LED will be ON when the USB is in device or...

_legacyfs_online_stmicro_images_0693W00000dDbZZQA0.png
RAnan.3 by Associate III
  • 1907 Views
  • 2 replies
  • 0 kudos

Crash when using bootloader to turn off protection

Can anyone confirm whether my understanding of the following behaviour is correct (and whether there's any way round it):When the built in bootloader has been entered by jumping to it from firmware (i.e. the BOOT0 pin is NOT pulled high), and the boo...

s_ by Associate III
  • 1639 Views
  • 2 replies
  • 0 kudos

STM32G473CBT freezes jumping to bootloader

I have a custom board using the STM32G473CBT6 MCU. BOOT0 is pulled-down by a 100k resistor and is used as GPIO (output) at runtime. The firmware is generated by CubeMX, with the addition of a C++ file for the 'user' application. The board works fine,...

StefanH by Associate III
  • 2048 Views
  • 2 replies
  • 0 kudos

STM32 Thread Safe Solution for Makefile Projects

I have a Makefile project for an STM32L4 using FreeRTOS that I started with STM32CubeMx. I'm trying to enable one of the Thread-Safe strategies for FreeRTOS. I have tried both strategy #4 and #5, but both of them jump to the error handler on the `S...

cvanbeek by Associate III
  • 1764 Views
  • 2 replies
  • 0 kudos

DFU When Booting from External Flash - STM32H730

Hi, I am working on a project with the STM32H730 that needs DFU capabilities for users to update software from a website. This project boots from an external flash memory due to large size requirements for program memory.Is there a way the DFU featur...

EPala.2 by Senior
  • 1697 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.