STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Attempting to run OctoSPI on STM32H753ZI

It might as well be a dumb question, but is it in any way possible to connect and communicate with a Octo SPI slave with the dual Quad-SPI interface available on the STM32H753ZI?Thanks and best!Sam.

sammie.k by Associate II
  • 5314 Views
  • 10 replies
  • 5 kudos

STM32 - update firmware from data stored in SRAM

I would like to remotely update the firmware of my STM32WLE5. I can transfer new binary file from the server to the STM's SRAM using my custom link only, which means I cannot utilize other native update procedures provided by STM, such as UART. Howev...

Foreen by Associate III
  • 1526 Views
  • 1 replies
  • 0 kudos

Resolved! LWIP Raw API udp_send() Cube MX HAL

Hi,LWIP: what is the difference between udp_send() and udp_sendto()?What are the use cases for each? The LWIP_RAW_CLIENT ECHO uses udp_send() but also uses udp_connect. Whereas udp_sendto() does not need to connect?Does anyone have example? Thanks

###### by Senior II
  • 4388 Views
  • 5 replies
  • 1 kudos

stm32h747i-disco HAL_UART_Init(&huart8) problem

 when i run if "(HAL_UART_Init(&huart8) != HAL_OK)" get blocked this code which part of code could wrong (RCC? SystemClock_Config?) ?(In stmcube ide no hay error en principio).static void MX_USART8_UART_Init(void){/* USER CODE BEGIN USART1_Init 0 *//...

wjian.2 by Associate III
  • 2228 Views
  • 4 replies
  • 0 kudos

Resolved! LWIP ISSUE stm32f769

hello, i have a problem. When I make my LWIP configurations and try to ping my development board over the computer, I see a different address, not the IP address I set for my card. What is the reason of this? Do you have an idea?When I ping the IP ad...

amorftor_0-1690269130893.png
amorftor by Associate II
  • 1511 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.