STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MKBOXPRO: Enabling 3A supply

Hi, I need to enable 3A supply on MKBOXPRO - referring to the attached schematic section; if I install 5.1K (1%?) pulldown resistors to GND, that are already provisioned for on R42,and R43, would that be all that I need to accomplish this?Another rel...

AVigh.1 by Associate II
  • 3249 Views
  • 2 replies
  • 0 kudos

STM32F411CE bootloader wrong USB VID/PID ?

When I hold BOOT0 while hitting Reset the Device boots up and configures the USB as VID/PID 0x0000/0x0002 but the STM32CubeProgrammer expects 0x0483/0xdf11.As far as I know the bootloader is in ROM (e.g. cannot be overwritten/damaged) so how can it b...

PRenn.1 by Associate III
  • 9205 Views
  • 10 replies
  • 1 kudos

STM32WL55 CM0+ is getting stuck

Dear forum,I have been working with the STM32WL55, using STM32Cube FW_WL V1.1.0.During the development phase I have tried to stress test the device with sending acknowledged LoRa messages one after the other. In order to ensure that I am not going to...

IAnas1_0-1695989037198.png IAnas1_2-1695989095287.png
IAnas.1 by Associate II
  • 1013 Views
  • 0 replies
  • 0 kudos

Can't downlaod STM32cubeMX or STM32cubeIDE

Hi, I just created a new profile and logged in to download STM32cubeMX and STM32cubeIDE. But no matter where I click on the download links, there is no response on the website. I have tied this in both Vivaldi and Edge browsers on Win11. I'm in the p...

OTA not able to powerup new firmware image

Hi,I am trying to perform OTA on STM32F413ZT6 using Seirra Wi-Fi module. The Sierra and MCU communicate over UART. Here the binary is downloaded by the WI-Fi from a server, further, it will send the binary to the MCU. The STM is responsible for writi...

saraiahd by Associate II
  • 839 Views
  • 0 replies
  • 0 kudos

Porting mcuboot to stm32 image unset?

Hi I have ported mcuboot to stm32 without os, following the https://interrupt.memfault.com/blog/mcuboot-overview. But I'm having problems and some things are not clear to me, hope someone can help me.By following the guide I implemented everything, a...

size.png bootloader2.png
suads by Associate III
  • 3552 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.