STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! A question on use timer and samples out

Good morning everyone,I'm at my first experience with STM and between guides and tutorials I'm learning many things.But I wanted to configure a 32bit TIM5 timer on my STM32F446 board, I would like my timer to calculate a sample every 0.000001s, only ...

Daddi by Associate
  • 1906 Views
  • 2 replies
  • 0 kudos

Resolved! RTC values don't change, although alarm is working

Hello,I am trying to use the RTC on a F401CCU6, but the values of the RTC don't change, and stay to what values I've set them in the IOC. I'm using the following function to get the time, and I read the values in the debugger. RTC_TimeTypeDef sTime;H...

Nescada_0-1704114514260.png
Nescada by Associate
  • 2305 Views
  • 2 replies
  • 0 kudos

Resolved! Changing PWM Mode during runtime

Hello, I am trying to write a routine, that takes an array of structures as input and sets the timer 1 parameters. This function is called after each overflow of timer 1. I turn off the respective channels, then set the parameters, as seen in the fol...

(Working) Audio Demo for STM32F746?

Hi all,I'm trying to get to know the STM32 world, and I have a STM32F746G-DISCOVERY board here. I've successfully tested a couple of TouchGFX things, and it seems quite neat.Now I want to test the possibility to output audio signals on the TRS output...

Resolved! STM32G474RE PA3/PC5 pin.

Hello,STM32G474RE is the processor model I use.I read ADC from pin PA3 and I read IO from pin PC5. So whether these pins are common pins in the processor hardware? How can I separate these two pins from each other?

SD Card

Does SanDisk Secure 4GB Class 4 SDHC Memory Card will support with STM32F732IE if not could you please suggest SD card with all specifications?

CMSIS HAL STACK TCP/IP BARE METAL (STM32H747I)

Hi community,one of project requirement we need to implement TCP IP protocol on STM32H747I DISC0.For our application we must use CMSIS (Common Microcontroller Software Interface Standard (CMSIS)) approved library so 1)LWIP is CMSIS approved or not?if...

Sandeepc by Associate
  • 1492 Views
  • 1 replies
  • 0 kudos

Resolved! Timer interrupts

HiI have a problem with the right priority setting, although I am not sure.The genelranie timer worked for me and refreshed the LCD screen every 375ms, but when I added interrupts for the ADC (needs to handle a potentiometer) then suddenly the TIM6 s...

1_debug.png 2_conf.png
grzeniux by Associate II
  • 3867 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.